DUG_4 Channel Relay_WI-00

Deleting a moment

  1. On the Moments page, locate the moment you want to delete.
  2. Slide left on the selected moment, it will show the option to edit and delete, tap DELETE.
  3. It will show a Warning pop-up, you can tap YES to delete the moment (A).
    NOTE: After deleting a moment, the device action can no longer be triggered.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.