DUG_Wiser Curtain Controller_WI-00

About the device

The Wiser Curtain Controller is a miniature micro module (hereinafter referred to as Puck), which is remotely controlled and designed to operate in AC mains. Dual curtain controller designed to control 2 blinds. It works with motorized roller blinds, IH11000200 is powered by a single-phase AC and provides precise positioning of blinds, so they can be set to the position you choose. The puck also operates as a repeater within the Z-Wave network it is associated, and uses the latest Z-Wave plus chip.

Devices controlled using curtain controller:

  • Curtains

  • Blinds

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.