DUG_Wiser Curtain Controller_WI-00

Creating a schedule

The device can be fully controlled by schedule. Once the schedule is set, the device operates at a given time.
  1. On the Home page, tap Schedule and tap to add the schedule.
    NOTE: If there is an existing schedule in the list then the add icon will be in white.
  2. Enter the name of the schedule (A).
  3. Go to the IF section and select the device you want under Device.
  4. Set the trigger condition using the slider, and set the action duration in Min(s) or Sec(s) or Hour(s) as per your need and, click OK to finish (B).
  5. Go to the THEN tab and choose the same device or a different device in the IF section under Device.
  6. Now select the Action Duration check box and enable the Toggle switch.
  7. Set the action duration in Min(s) or Sec(s) or Hour(s) as per your need.-For example. 15 Min(s) (C).
  8. Go to the WHEN tab and select the TIME OF ACTION (D) and tap SAVE (E).
The created schedule will be available in the Schedule page list.

For more information on creating a schedule, refer to the video How to create a schedule
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.