DUG_Wiser Curtain Controller_WI-00

Changing the device location

Using the Wiser India app, add the puck to any room (such as living room, bedroom, kitchen etc).
  1. On the Home page, tap .
  2. On the device page, select the device for which you wish to assign a different location.
  3. My Device (A).
  4. Select the Assigned to room to assign the puck to an existing room or a new room (B).
    NOTE: My Device is the name given to the device by the user. Any name can be assigned by editing in the device option.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.