DUG_Wiser Curtain Controller_WI-00

Pairing the device

Using the Wiser India app, pair your puck with the Gateway Hub to access and control the puck.

To pair the puck:
  1. On the Home page, tap Device.
  2. Tap Add > Schneider Electric > 4 Channel Relay (A).
    The next screen shows the joining process of Puck.
    NOTE:
    The gateway generates a "beep“ sound.
  3. Trigger the device by pressing on the Programming button on the back of the device and make sure the LED blinks green.
    NOTE: If the puck device blinks Red LED then it means that the device is not added to any gateway.
  4. Wait for a few seconds until the LED turns green. You can also see in the app that the device is joined.
  5. Tap Next to enter the name of the device and assign the device to a new room or an existing room.
    The Puck is now listed under Device page.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.