DUG_Wiser Curtain Controller_WI-00

Manual operation

When the puck is connected to a bell button switch, the shutter can be controlled manually.

  • Press and hold the bell button switch to open/close the shutter gradually.


NOTE: When the puck is installed inside the wall box, the status LED is not visible while using the puck.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.