DUG_Wiser Fan Speed Controller_WI-00

Creating a moment

A Moment allows you to group multiple actions that are usually done together.
Using the Wiser India app, you can create moments based on your needs.
  1. On the Home page, go to Moments > + to create a moment (A).
  2. Tap Enter the name (B), type the name of the moment and select the icon and tap SAVE (C).
  3. Tap on > beside the created moment name (D).
  4. Tap Device and select the device to set the condition (E), tap Continue (F).
  5. Set the condition and tap OK to finish. For example: Select Fan and choose the fan speed as 2 and tap OK to finish (G).
    NOTE: To check the moments, turn off all the devices and run the scene.

  6. To run the moments, tap Moments and tap on the created moment icon (H).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.