DUG_Wiser Fan Speed Controller_WI-00

LED indication

Pairing the device

User Action

LED Indication

Status

>Short press the programming button 3 times.

Both red and green LED’s glows constantly.

Pairing mode is active. When pairing is completed, LED blinks green continuously.

Resetting the device

User Action

LED Indication

Status

>Short press the programming button 3 times or hold it down once for > 10 s.

LED blinks red once per second.

The device is in reset mode. The device then restarts indicating that the device is ready for pairing.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.