DUG_Wiser Fan Speed Controller_WI-00

Removing the device

Using the Wiser India app, you can remove a device from the device list.


To remove the device:
  1. On the Home page, tap Device.
  2. Tap Remove > Other Z-Wave device > YES (If you heard the beep sound).
    TIP: Alternatively, on the Home page, tap , tap on the device you want to delete and tap Force to remove or replace > Remove.
    NOTE:
    • Removing the device will reset the Puck. After reset the LED turns RED indicating that the Puck is ready to pair with another network.

    • For more information, please refer to the video: How to remove the device.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.