2110CT9701

Accessories

A wide variety of accessories are available for field or factory installation of I-Line panelboards.

Equipment Ground Bars

Equipment Ground Bar (Catalog No.

PK32DGTA)

Equipment ground bars mount in the panelboard box to provide convenient termination of equipment grounding conductors. They are available in copper or aluminum.

Box Extensions

Typical Box Extensions

Box extensions provide additional end gutter for feeding cables into the end of the cabinet; they are UL/CSA Listed. Several extension heights are available as add-on kits in the field as shown below. In addition custom extensions are available in Factory Assembled panelboards.

Interior Type

Extension

HCP-SU

9 in.

HCJ

9 in.

HCP

12 in.

HCR-U

6 in.

HCR-U

12 in.

Blank Fillers/Extensions

Blank Fillers
(Catalog Nos.

HNM4BL Qty. 5 per box and HNM1BL Qty. 3 per box)

Blank fillers are required to cover unused mounting space in I-Line panelboards. Blank Extensions are used to fill the gap between the filler or circuit breaker and the panelboard deadfront.

Blank Extensions

Service Entrance Barriers

Panelboards are suitable for use as service equipment if equipped with an integral main circuit breaker and service entrance barrier kit. Vertical mains or group mounted mains can be a service entrance main circuit breaker. There are separate Service Entrance Barrier versions available for US and Canada. In the US, under the 2017 UL67 and NFPA70 standards there is an exception when not more than six main disconnecting means are provided and the panelboard is not used as a lighting and appliance branch circuit panelboard that service entrance barriers are not required. The 2020 edition of the US National Electrical Code (NEC) no longer allows two to six service disconnecting means to be in the same panelboard enclosure thereby eliminating the above exception for states that have adopted the 2020 NEC.

NOTE: Service Entrance option for Canada must be installed in the SE factory per Canadian Codes.

Drip Hoods

Drip Hood

Primarily used for NEMA 2 applications in Canada these hoods are intended for use on surface mounted boxes only. The Drip Hoods are designed to fit on the outside of the boxes. The Drip Hood will increase the enclosure rating of the box from Type 1 to Type 2. Reference Instruction Bulletin 80043-401-03.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.