6045IB2401

Typical Control Circuit

Typical Control Circuit-Electrically Operated SEM Control Circuit

Operation of Switch

  1. The switch closes if the closing springs have been charged electrically or manually.

  2. The closing circuit has continuity when the closing springs are charged, the switch is open and no continuous trip signal is applied. Applying a close signal energizes the close coil, Y2. It discharges the closing springs, closing the switch. When the switch closes. A5/a and A5/b change state.

  3. A5/a closing allows continuity in the trip circuit. A5/b opens, opening the close circuit.

  4. Applying a trip signal energizes the trip coil, Y1. It discharges the opening springs, opening the switch. When the switch opens, A5/a and A5b change state.

  5. Spare A5/a and A5/b contacts indicate the breaker state. A5/a closes when the switch closes. A5/b closes when the switch opens.

Legend

F1 Cartridge Fuse, KLM3
K1 Anti-Pump Relay
K2 Control Relay
M Charging Motor
51, 53-56 Switch Position Auxiliary Switch Contacts (A5/a)
52, 57-59 Switch Position Auxiliary Switch Contacts (A5/b)
510, 11, 12 Grounding Switch Position Auxiliary Switch Contacts
513 Load Break Switch Operating Lever Actuated Contact
514 Grounding Switch Operating Lever Actuated Contact
515, 16 Charging Limit Switch Contacts
517 End of Charge Motor Contact
518, 19 Blown/Missing Fuse Indiction/Interlock
520 Control Depress Contact
521 Lock Auxiliary Switch
TBM Terminal Block
Y1 Trip Coil
Y2 Close Coil
3 Auxiliary Blown/Missing Fuse Relay (Instantaneous and TDE)
NOTE:
  • Switch shown in the open state with closing springs discharged.

  • Grounding switch shown in the open state.

  • Some terminal points not shown for simplicity.

  • Switch wiring diagram is 44044-177.

  • Destination wire markers without wire numbers are used in mechanism.

  • Diodes are on DC control power module only.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.