D4035235-00

ADVC3 Firmware Update Policy

Firmware update is recommended in order to benefit from the latest features, enhancements and bug fixes. Use this release note to determine whether an update to the latest version of the ADVC3 firmware is relevant for your application.

NOTE: Only update the firmware to the latest version if your application requires the new features, enhancements, or relevant bug fixes.

Configuration Software

Use the WSOS 5.16.38 software to update the firmware for the ADVC3 system.

ADVC3 Firmware Update

The firmware of the ADVC3 system is delivered in an ADVC3 package. The firmware can be updated by using WSOS.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.