PowerLogicTM Advanced Controller (ADVC)
The PowerLogic™ ADVC range is a controller for Automatic Circuit Reclosers (ACRs) and Automatic Sectionalisers (AS).
ACR consists of an ADVC Controller and circuit breaker switchgear connected by an umbilical control cable; designed to interrupt high fault currents.
An AS also consists of a PowerLogic ADVC and a compatible switchgear connected by an umbilical control cable. The switchgear can be either a Load Break Switch (LBS), which is not designed to interrupt high fault currents, or a circuit breaker.
The design features of PowerLogic ADVC are as follows:
-
Outdoor pole-mounted use
-
Cubicle vents have screens help to prevent vermin entry
-
The cubicle door has a seal
-
Rain shield helps protect Miniature Circuit Breakers (MCBs) if the cubicle door is open for a short period of time during light rain during maintenance
-
All electronic modules and the cubicle itself are IP65 rated
-
Battery heater mat can be supplied if required.
Condensation inside the cubicle may occur in certain conditions, such as tropical storms, but it only forms on metal surfaces and is harmless. Water drains out or evaporates through ventilation and self-heating.