D4035235-00

WSOS Software Update Policy

Software update is recommended to benefit from the latest features, enhancements and potential bug fixes. Use this release note to determine whether an update to the latest version of the WSOS software is relevant for your application.

NOTE: Update the software to the latest version before updating to the new firmware version. Older software versions may not support new features or enhancements.

WSOS Software Update

The WSOS software is provided in an installer executable. To install or update WSOS, run the installer; this will either perform a first-time installation or replace the previous version with the latest one.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.