D4035235-00

Windows Switchgear Operating System (WSOS)

WSOS Software application runs on Microsoft Windows® for management, control, and monitoring of PowerLogic ADVC.

WSOS provides full access to switchgear functions: opening/closing, protection settings and communication parameters through accessing measurement and analytical data.

By using a desktop or a portable PC, engineers can manage many/multiple devices remotely through a communication link or locally through a serial, USB or Ethernet connection.

WSOS provides:

  • Local language support

  • Advanced controller support

  • SCADA communications capture tool

  • Controller firmware loading

  • Switchgear explorer

  • Launch pad

  • Switchgear status

  • Event log and filtering

  • Feature selection page

  • Setting pages.

WSOS also supports:

  • Online and offline management of all protection settings

  • Tripping and Closing of the switchgear and other operator control functions

  • Uploading of historical data (for example, event record or demand measurements) to the computer, which can be taken away and processed elsewhere.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.