D4035235-00

Software Version 5.16.38

WSOS User Interface changes

This section details changes to WSOS User Interface.

Jira DAN

Development

Change

Image

DAN-1599

WSOS - Error loading firmware when setting text manually

Users can now enter the firmware path manually without errors

-

DAN-1601

WSOS - Invalid Point List Link

WSOS now links to the correct Point List

-

DAN-2007

Fault Current DNP3 Analog Value when in Alarm Mode

History Logs now display peak current values when Alarm Mode is active

-

DAN-2077

WSOS- Platform options appear at Product selection

Product Selection when creating a file works properly, WSOS helps prevent selection of incompatible combinations of Platform+Controller, Range+Operator, and Interface+Firmware Version

DAN-2240

WSOS - ROCOF UOF Online Help correction

Changed the wording to be more accurate

-

DAN-2287

WSOS - Online help for PMSet UR Series

WSOS Online Help now includes references to PMSet UR Series

-

DAN-2297

WSOS - Allows to downgrade to a FW where UR Series switchgear is unknown

WSOS now prompts users with a confirmation message if they want to downgrade to a firmware version that does not support UR Series when trying to do it with a CAPE connected to UR Series

DAN-3220

WSOS - Removal of "Hybrid Mode" and "TEF" in feature selection

WSOS no longer displays TEF, Hybrid Mode selection and other settings

-

DAN–2601

ADVC3 - Pick Up multiplier 331 Point List

Users can now select Pickup Multiplier in the DNP3 Mapping (331 Point List)

-

DAN–1593

ADVC3 - Inrush Restraint 331 Point List

Users can now select Inrush Restraint in the DNP3 Mapping (331 Point List)

-

Multiple

PMSet UR Series

WSOS now displays PMSet UR Series features and related information in different WSOS windows

-

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.