D4035235-00

Installation

Installation Preparation

Administrator or equivalent privilege is required to install the WSOS software on PC.

Installation Language

The language of the Installation dialog box and the installed version is derived from the user language setting pre-defined by the operating system.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.