NVE75505

Appendix A

Zelio™ Smart Relay Ladder Logic

The Zelio Smart Relay controls the power converter’s output contactor and the bypass contactor when Bypass (Mod Y10) is selected. Zelio Smart Relay Programcontains a diagram of the default Zelio Smart Relay program. See Zelio Smart Relay Ladder Logic Timers for a timing chart, Zelio Smart Relay Discrete Inputs for the discrete inputs, and Zelio Smart Relay Discrete Outputs for the discrete outputs.

Custom requests may result in a program that differs from the one illustrated in Zelio Smart Relay Program. If you have requested custom programming, review the drawings supplied with the process drive.

Zelio Smart Relay Ladder Logic Timers

Timer Description Function Time (s)
T1 Power on delay A: Active, control held down 6
T2 Open delay C: Off delay 2
T3 AFC run delay A: Active, control held down 5
T4 AFC contactor time delay A: Active, control held down 3
T5 Bypass contactor time delay A: Active, control held down 3
T6 Drive trip signal delay A: Active, control held down 2
T7 Start with Line contactor B: On pulse one shot 6

Zelio Smart Relay Discrete Inputs

Physical Inputs Function Comment
I1 Discrete input HOA in hand mode
I2 Discrete input HOA in auto mode
I3 Discrete input Auto mode input
I4 Discrete input Drive R1 (trip)
I5 Discrete input Drive R2 (run)
I6 Discrete input AFC/off/Bypass in AFC
I7 Discrete input AFC/off/Bypass in Bypass
I8 Discrete input Test/Normal mode switch
I9 Discrete input Overload relay trip state

Zelio Smart Relay Discrete Outputs

Physical Outputs Function Comment
Q1 Discrete output AFC contactor
Q2 Discrete output Bypass contactor
Q4 Discrete output AFC run command
Q6 Discrete output Start push button seal (Mod B11)

Zelio Smart Relay Program

Zelio Smart Relay Program

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.