NVE92630

Appendix A - Zelio™ Smart Relay Ladder Logic

The Zelio Smart Relay controls the power converter’s output contactor and the bypass contactor when Mod Y10, Bypass, is selected. Zelio Smart Relay Program contains a diagram of the default Zelio Smart Relay program. See Zelio Smart Relay Ladder Logic Timers for a timing chart, Zelio Smart Relay Discrete Inputs for the discrete inputs, and Zelio Smart Relay Discrete Outputs for the discrete outputs.

Custom requests may result in a program that differs from the one illustrated in Zelio Smart Relay Program. If you have requested custom programming, review the drawings supplied with the process drive.

Zelio Smart Relay Ladder Logic Timers

Timer

Description

Function

Time (s)

T1

Power on delay

A: Active, control held down

6.0

T2

Open delay

C: Off delay

2.0

T3

AFC run delay

A: Active, control held down

5.0

T4

AFC contactor time delay

A: Active, control held down

3.0

T5

Bypass contactor time delay

A: Active, control held down

3.0

T6

Drive trip signal delay

A: Active, control held down

2.0

T7

Start with Line contactor

B: On pulse one shot

6.0

Zelio Smart Relay Discrete Inputs

Physical Inputs

Function

Comment

I1

Discrete input

HOA in hand mode

I2

Discrete input

HOA in auto mode

I3

Discrete input

Auto mode input

I4

Discrete input

Drive R1 (trip)

I5

Discrete input

Drive R2 (run)

I6

Discrete input

AFC/off/Bypass in AFC

I7

Discrete input

AFC/off/Bypass in Bypass

I8

Discrete input

Test/Normal mode switch

I9

Discrete input

Overload relay trip state

Zelio Smart Relay Discrete Outputs

Physical Outputs

Function

Comment

Q1

Discrete output

AFC contactor

Q2

Discrete output

Bypass contactor

Q4

Discrete output

AFC run command

Q6

Discrete output

Start push button seal (Mod B11)

Zelio Smart Relay Program

Zelio Smart Relay Program (continued)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.