Appendix A - Zelio™ Smart Relay Ladder Logic
The Zelio Smart Relay controls the power converter’s output contactor and the bypass contactor when Mod Y10, Bypass, is selected. Zelio Smart Relay Program contains a diagram of the default Zelio Smart Relay program. See Zelio Smart Relay Ladder Logic Timers for a timing chart, Zelio Smart Relay Discrete Inputs for the discrete inputs, and Zelio Smart Relay Discrete Outputs for the discrete outputs.
Custom requests may result in a program that differs from the one illustrated in Zelio Smart Relay Program. If you have requested custom programming, review the drawings supplied with the process drive.
Zelio Smart Relay Ladder Logic Timers
|
Timer |
Description |
Function |
Time (s) |
|---|---|---|---|
|
T1 |
Power on delay |
A: Active, control held down |
6.0 |
|
T2 |
Open delay |
C: Off delay |
2.0 |
|
T3 |
AFC run delay |
A: Active, control held down |
5.0 |
|
T4 |
AFC contactor time delay |
A: Active, control held down |
3.0 |
|
T5 |
Bypass contactor time delay |
A: Active, control held down |
3.0 |
|
T6 |
Drive trip signal delay |
A: Active, control held down |
2.0 |
|
T7 |
Start with Line contactor |
B: On pulse one shot |
6.0 |
Zelio Smart Relay Discrete Inputs
|
Physical Inputs |
Function |
Comment |
|---|---|---|
|
I1 |
Discrete input |
HOA in hand mode |
|
I2 |
Discrete input |
HOA in auto mode |
|
I3 |
Discrete input |
Auto mode input |
|
I4 |
Discrete input |
Drive R1 (trip) |
|
I5 |
Discrete input |
Drive R2 (run) |
|
I6 |
Discrete input |
AFC/off/Bypass in AFC |
|
I7 |
Discrete input |
AFC/off/Bypass in Bypass |
|
I8 |
Discrete input |
Test/Normal mode switch |
|
I9 |
Discrete input |
Overload relay trip state |
Zelio Smart Relay Discrete Outputs
|
Physical Outputs |
Function |
Comment |
|---|---|---|
|
Q1 |
Discrete output |
AFC contactor |
|
Q2 |
Discrete output |
Bypass contactor |
|
Q4 |
Discrete output |
AFC run command |
|
Q6 |
Discrete output |
Start push button seal (Mod B11) |