QGH27523

Operation Instructions

DANGER
hazard of electric shock, explosion, or arc flash
  • Before working on this equipment, turn off all power supplying it and perform the “DC Bus Voltage Measurement Procedure” in bulletin NHA60269, Drives Systems Installation and Maintenance.
Failure to follow these instructions will result in death or serious injury.
DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • This equipment must be installed and serviced only by qualified personnel.
  • Qualified personnel performing diagnostics or troubleshooting that requires electrical conductors to be energized must comply with:
  • NFPA® 70 E®Standard for Electrical Safety Requirements for Employee Workplaces®
  • CSA Z462 – Workplace Electrical Safety
  • OSHA Standards – 29 CFR Part 1910 Subpart S Electrical
  • NOM-029-STPS – Maintenance of Electrical Installation in the Workplace, Safety Conditions
  • Other national and local electrical codes that may apply
Failure to follow these instructions will result in death or serious injury.
DANGER
hazard of electric shock, explosion, or arc flash
  • Properly ground the enclosed drive before applying power.
  • Close and secure the enclosure doors before applying power.
  • Certain adjustments and test procedures require that power be applied to this enclosed drive. Exercise extreme caution as hazardous voltages exist. The enclosure door must be closed and secured while turning on power or starting and stopping this enclosed drive. Always follow practices and procedures from NFPA® 70E™, CSA Z462, NOM-029-STPS, and other applicable regulations defining safe electrical work practices.
Failure to follow these instructions will result in death or serious injury.
WARNING
Loss of Control
  • The designer of any control scheme must consider the potential failure modes of control paths and, for certain critical control functions, provide a means to achieve a safe state during and after a path failure. Examples of critical control functions are emergency stop and over travel stop.
  • Separate or redundant control paths must be provided for critical control functions.
  • System control paths may include communication links. Consideration must be given to the implications of anticipated transmission delays or failures of the link.*
  • Each implementation of the ATV680 Process Drive must be individually and thoroughly tested for proper operation before being placed into service.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
CAUTION
INCOMPATIBLE LINE VOLTAGE
Before powering up and configuring the equipment, ensure that the line voltage is compatible with the supply voltage shown on the enclosed drive nameplate. The enclosed drive may be damaged if the line voltage is not compatible.
Failure to follow these instructions can result in injury or equipment damage.

WARNING: This product can expose you to chemicals including lead and lead compounds, which are known to the State of California to cause cancer and birth defects or other reproductive harm. For more information go to www.P65Warnings.ca.gov.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.