QGH27523

Programming and Setup

DANGER
hazard of electric shock, explosion, or arc flash
Read and understand the instructions in bulletin NHA60269, Drives Systems Installation and Maintenance, before performing any procedures in this bulletin.
Failure to follow these instructions will result in death or serious injury.

Factory Settings

If the power converter has been replaced or reset to the factory settings, you may need to adjust some parameter values. Parameter settings are included in the documentation provided with the equipment.

Adjusting the PowerPacT™ Circuit Breaker Trip Settings

Some circuit breakers have trip settings that may need adjustment according to the application and motor type. For more information on trip setting adjustment, refer to the circuit breaker instruction bulletin provided with the equipment, or available for download from the Technical Library at www.se.com.

PowerPacT J FLA and Im Dial

Overload Relay Adjustment

Always verify that the overload relay setting does not exceed the motor full load current or rated power converter current found on the nameplate, whichever is less.

Overload Relay Adjustment Range for Full-Voltage Bypass Operation provides the adjustment range for overload relays according to horsepower rating and voltage. Contact Schneider Electric if the adjustment range does not meet the intended application.

Overload Relay Adjustment Range for Full-Voltage Bypass Operation

hp

460 V

150

132–220

200

200–330

250

200

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.