Add Features to Reports
Use the settings below to include your custom feature in specific reports. This topic does not include configuration for the Patch Panel Connection Report. You can configure one of two versions of the Patch Panel Connection Report: Flexible or Original.
View the Configure Fiber Manager Reports topic for additional report configuration details.
Glass Report
Add the following field names to linear features you want to appear in the Glass Report. The feature or object must be a linear (complex edge) object type which contains connectable objects and tracks length (e.g., FiberOpticCable).
-
The Example Field Name, Data Type and Domain columns contain values entered when the feature is created. If using the worksheet, record these values in Table 5.
-
The Field Model Name column contains values entered in the ArcFM Properties Manager on the Field Model Names tab. If using the worksheet, record these values in Table 5.
|
Example Field Name |
Data Type |
Domain |
Field Model Name |
|---|---|---|---|
|
NumberOfStrands |
Long Integer |
NUMBEROFSTRANDS |
|
|
OverheadUnderground |
Text |
Fiber Overhead Underground |
OVERHEADUNDERGROUND |
|
SheathType |
Text |
SHEATHTYPE |
Schematic Reports
If you want the attributes of an object to be accessible in the Schematic reports, then create a field and assign it the field model name SCHEMATICEXPORTATTRIBUTE. Once the custom feature is configured, you must also configure (or reconfigure, it if it already exists) the schematic (circuit or splice) to add your custom feature.
|
Example Field Name |
Data Type |
Field Model Name |
|---|---|---|
|
Any field |
Any, except date |
SCHEMATICEXPORTATTRIBUTE |