Define Points and Lines
If you haven't already, determine your feature's geometry (Table 3 on the worksheet): point or line. If you have a line feature, create it as an ArcFM Complex Edge feature. If you have a point feature, create it as an ArcFM Simple Junction feature.
Point Feature Settings
Point features can have certain properties (e.g., splitting fiber lines) which use specific class model names, fields and autoupdaters. The following table describes the class model names, fields and autoupdaters used by point features.
Using the Settings for Point Features Table
-
The Example Field Name and Data Type columns contain values entered while creating the feature. If using the worksheet, record these values in Table 5.
-
The Field Model Name column contains values entered in the ArcFM Properties Manager on the Field Model Names tab. If using the worksheet, record these values in Table 5.
-
The Class Model Name column contains values entered in the ArcFM Properties Manager on the Model Names tab. If using the worksheet, record these values in Table 4.
-
The Object Autoupdaters row contains the object autoupdaters entered in the ArcFM Properties Manager on the Object Info tab. If using the worksheet, record these values in Table 6.
Settings for Point Features Table
|
Function |
Settings |
|||
|---|---|---|---|---|
|
Example Field Name |
Data Type |
Field Model Name |
Class Model Name |
|
|
Modifiable by Location Editor |
LOCATIONEDITABLE |
|||
|
Represents length but does not split cables |
Length |
Double |
POINTLENGTH |
|
|
Object Autoupdaters:
|
||||
|
Splits cable lines |
||||
|
Object Autoupdaters:
|
||||
|
Splits cable lines and has editable connections |
FIBERCONNECTIONCONTAINER |
|||
|
Object Autoupdaters:
|
||||
|
Represents a change in a linear feature's field |
TRANSITIONPOINT (Transition points are ignored when running the Allocation Report) |
|||
|
Object Autoupdaters:
|
||||
Line Feature Settings
Linear features can have certain properties, such as appearing in the glass report, which use specific class model names, fields and autoupdaters. The following table describes the class model names, fields and autoupdaters needed for line features with the following functions.
-
The Example Field Name, Data Type, and Domain columns contain values entered when creating the feature. If using the worksheet, record these values in Table 5.
-
The Assign Field Model Name column contains values entered in the ArcFM Properties Manager on the Field Model Names tab. If using the worksheet, record these values in Table 5.
-
The Assign Class Model Name column contains values entered in the ArcFM Properties Manager on the Model Names tab. If using the worksheet, record these values in Table 4.
-
The Object Autoupdaters row contains the object autoupdaters entered in the ArcFM Properties Manager on the Object Info tab. If using the worksheet, record these values in Table 6.
Settings for Line Features Table
|
Function |
Settings |
|||
|---|---|---|---|---|
|
Example Field Name |
Data Type |
Field Model Name |
Class Model Name |
|
|
Modifiable by Location Editor |
LOCATIONEDITABLE |
|||
|
Contains connectable objects and tracks length |
EndFootStamp |
Long Integer |
ENDFOOTSTAMP |
|
|
StartFootStamp |
Long Integer |
STARTFOOTSTAMP |
||
|
FieldNotesLength |
Double |
FIELDNOTESLENGTH |
||
|
SheathLengthSource |
Text |
SHEATHLENGTHSOURCE (assign the "Fiber Optic Cable Length Source" domain to this field) |
||
|
TwistFactor |
Double |
TWISTFACTOR |
||
|
GlassLength |
Double |
GLASSLENGTH |
||
|
SegmentGlassLength |
Double |
SEGMENTGLASSLENGTH |
||
|
SheathLength |
Double |
SHEATHLENGTH |
||
|
SegmentLength |
Double |
SEGMENTLENGTH |
||
|
Object Autoupdaters:
|
||||