F_PATCHPANEL
-
ObjectID fields are automatically created (by Esri) when you create the schema.
-
GlobalID fields are required by Fiber Manager and are created with Esri's Add Global ID tool (Manage > Add Global IDs).
-
Tables must be versioned for an SDE database. See Esri’s documentation for more information about versioning tables.
-
Tables must also be converted to ArcFM Objects.
-
In ArcGIS applications, there are four numeric data types: Short Integer, Long Integer, Float, and Double. The choices reflect a balance between minimizing storage space while still allowing enough range and precision for the field to be useful. For example, because lengths typically have decimals, these fields are assigned either Float or Double.
In the table below, any field set to integer does need to be either a Short or Long Integer, as these fields cannot contain decimals. So, the decision comes down to the minimum and maximum values you need for the field:
-
Short Integer Storable Range: -32,768 to 32,767
-
Long Integer Storable Range: -2,147,483,648 to 2,147,483,647
So, as an example, would you ever have more than 32,767 patch panels on a single rack? No. So, the RackPosition field could be a Short Integer. Conversely, foot or meter stamps along a cable could easily exceed 32,767. So, CableMarking fields should be a Long Integer. Our integer recommendations err on the side of more range and usefulness, but your company could decide to change a Long Integer to a Short Integer (or a Double down to a Float) if you knew the maximum values would never exceed the types’ upper threshold.
-
Alias: Patch Panel
|
Field |
Data Type |
Default Value |
Domain |
Length/Precision |
|---|---|---|---|---|
|
DefaultCardWidth Alias: Width |
Short Integer |
|||
|
FiberChildClassModelName Alias: Fiber Child Class Model Name |
Text |
50 |
||
|
FiberParent Alias: Fiber Parent |
Guid |
|||
|
FiberParentClassModelName Alias: Fiber Parent Class Model Name |
Text |
50 |
||
|
Name |
Text |
50 |
||
|
NumberOfCardColumns Alias: Number of Columns |
Short Integer |
|||
|
NumberOfCardRows Alias: Number of Rows |
Short Integer |
|||
|
RackSides Alias: Sides of Rack Shown On |
Text |
Fiber Connection Location |
50 |
|
|
SlotOrientation Alias: Orientation |
Text |
Fiber Slot Orientation |
50 |
|
|
ThisFiberClassModelName Alias: This Fiber Class Model Name |
Text |
PatchPanel |
50 |
Field Display
Primary Display Field: Choose this field in the ArcFM Properties Manager. The chosen field is displayed when using ArcFM tools such as the ArcFM Locator and ArcFM Attribute Editor. Your company can choose the most useful field to display for the end users. If the chosen field is null for the selected or identified features, the display field defaults to the ObjectID.
Because this choice also determines what is displayed on connection reports, Name is recommended.
Model Names
FIBERDATATABLESOURCE, FIBERGRIDABLECONTAINER, FIBERGRIDABLEOBJECT, FIBEROBJECT, PATCHPANEL
Field Model Names
DefaultCardWidth: FIBERGRIDDEFAULTWIDTH
FiberChildClassModelName: FIBERCHILDCLASSMODELNAME
FiberParent: FIBERPARENT
FiberParentClassModelName: FIBERPARENTCLASSMODELNAME
GlobalID: GLOBALID
Name: FIBERCIRCUITREPORTFIELD, FIBEROTDRREPORTFIELD, FIBERTRACEREPORTFIELD, SCHEMATICEXPORTATTRIBUTE
NumberOfCardColumns: FIBERNUMBERGRIDCOLUMNS
NumberOfCardRows: FIBERNUMBERGRIDROWS
RackPosition: FIBERGRIDPOSITION
RackSides: FIBERFACETSCONTAINEDBY
SlotOrientation: SLOTORIENTATION
ThisFiberClassModelName: THISFIBERCLASSMODELNAME
AutoUpdaters
On Feature Delete: ArcFM Fiber Object Deleted
Field Autoupdaters
ChangeDate — On Feature Update: ArcFM Current Date
ChangeUser — On Feature Update: ArcFM Login User Name
CreationDate — On Feature Create: ArcFM Current Date
CreationUser — On Feature Create: ArcFM Login User Name