F_CIRCUIT
-
ObjectID fields are automatically created (by Esri) when you create the schema.
-
GlobalID fields are required by Fiber Manager and are created with Esri's Add Global ID tool (Manage > Add Global IDs).
-
Tables must be versioned for an SDE database. See Esri’s documentation for more information about versioning tables.
-
Tables must also be converted to ArcFM Objects.
-
In ArcGIS applications, there are four numeric data types: Short Integer, Long Integer, Float, and Double. The choices reflect a balance between minimizing storage space while still allowing enough range and precision for the field to be useful. For example, because lengths typically have decimals, these fields are assigned either Float or Double.
In the table below, any field set to integer does need to be either a Short or Long Integer, as these fields cannot contain decimals. So, the decision comes down to the minimum and maximum values you need for the field:
-
Short Integer Storable Range: -32,768 to 32,767
-
Long Integer Storable Range: -2,147,483,648 to 2,147,483,647
So, as an example, would you ever have more than 32,767 patch panels on a single rack? No. So, the RackPosition field could be a Short Integer. Conversely, foot or meter stamps along a cable could easily exceed 32,767. So, CableMarking fields should be a Long Integer. Our integer recommendations err on the side of more range and usefulness, but your company could decide to change a Long Integer to a Short Integer (or a Double down to a Float) if you knew the maximum values would never exceed the types’ upper threshold.
-
Alias: Circuit
|
Field |
Data Type |
Default Value |
Domain |
Length/Precision |
|---|---|---|---|---|
|
CircuitChannel Alias: Channel |
Text |
Fiber Circuit Channel |
50 |
|
|
CircuitLength Alias: Length |
Double |
|||
|
CircuitName Alias: Name |
Text |
50 |
||
|
CircuitType Alias: Type |
Text |
Fiber Circuit Type |
50 |
|
|
CircuitStatus Alias: Status |
Text |
Fiber Circuit Status |
50 |
|
|
FiberCircuitGraph Alias: Fiber Circuit Graph |
Text |
Less than 4,000, if possible
IMPORTANT:
This field contains a character-based tracking method to understand the connections within the circuit. It is automatically populated and maintained by the application. A short circuit would look something like: {“start”:0,“edges”:[[0,1],[1,2],[2,3]]} The above circuit is 39 characters. Ideally, this field’s length would be no more than the longest circuit’s character count in your system because the shorter the length, the better the performance of Circuit Manager. We recommend you trace and create your longest circuit, find its character length in this field, and use that number + a small buffer of additional characters as the global length for this field. Finally, if the length exceeds 4,000 characters, your enterprise database (SQL or Oracle) converts this field to a BLOB. While that improves storage efficiency, it slows end user performance while using Circuit Manager, especially while in an editing session. That is why the recommendation is less than 4,000, if possible. |
||
|
FiberCircuitHeaderClass Alias: Fiber Circuit Header Class |
Text |
50 |
||
|
FiberCircuitHeaderGlobalID Alias: Fiber Circuit Header Global ID |
Guid |
|||
|
FiberCircuitTraceStyle Alias: Fiber Circuit Trace Style |
Long Integer |
|||
|
FiberLambda Alias: Wavelength (nm) |
Double |
|||
|
GlobalID Alias: Global ID |
Guid |
Field Display
Primary Display Field: Choose this field in the ArcFM Properties Manager. The chosen field is displayed when using ArcFM tools such as the ArcFM Locator and ArcFM Attribute Editor. Your company can choose the most useful field to display for the end users. If the chosen field is null for the selected or identified features, the display field defaults to the ObjectID.
Because this choice also determines what is displayed on the Circuit Trace Report, CircuitName is recommended.
Model Names
FIBERCIRCUITTABLE
Field Model Names
CircuitChannel: CIRCUITCHANNEL
CircuitLength: CALCULATEDFIBERCIRCUITLENGTH
CircuitName: FIBERCIRCUITNAME
CircuitStatus: FIBERSTATUS
CircuitType: CIRCUITTYPE
FiberCircuitGraph: FIBERCIRCUITGRAPH
FiberCircuitHeaderClass: FIBERCIRCUITHEADERCLASS
FiberCircuitHeaderGlobalID: FIBERCIRCUITHEADERGLOBALID
FiberCircuitTraceStyle: FIBERCIRCUITTRACESTYLE
FiberLambda: FIBERLAMBDA
GlobalID: GLOBALID
Object AutoUpdaters
On Feature Create — ArcFM Fiber Calculated Circuit Length
On Feature Update — ArcFM Fiber Calculated Circuit Length
Field Autoupdaters
ChangeDate — On Feature Update: ArcFM Current Date
ChangeUser — On Feature Update: ArcFM Login User Name
CreationDate — On Feature Create: ArcFM Current Date
CreationUser — On Feature Create: ArcFM Login User Name