Fiber Trace Troubleshooting
You must properly configure Fiber Manager before its tracing tools function correctly. Most tracing problems arise from the misconfiguration of the Fiber Manager's flexible data model.
The following sections describe the most common sources of misconfiguration:
Missing Field Model Names
Every fiber object must have the following field model names assigned:
Learn more about required model names.
Relationship autoupdaters not assigned
Check to make sure that for all parent-child relationships, the ArcFM Update Fiber Parent Field autoupdater is assigned to the On Relationship Created event.
Default values
All fiber objects must have a default value for THISFIBERCLASSMODELNAME.
When using flexible fiber features, the default value can be anything you choose, so long as it matches the model name assigned to the fiber object class. For example, if you want the default value of FIBEROPTICCABLE to be FOC, you would follow these steps:
- Right-click the geodatabase and select Properties.
- In the Domains tab, create the FOC model name. Click OK.
- Right-click the FiberOpticCable feature class and select ArcFM Properties Manager.
- In the Model Names tab, assign the new model name. Click OK.
- Right-click the feature class and select Properties.
- Assign FOC as the default value for THISFIBERCLASSMODELNAME. Click OK.