Assign Model Names and AUs
To assign model names and autoupdaters, right-click the new feature or object, then select ArcFM Properties Manager. After you've finished assigning settings on a tab, click the Apply button. Some autoupdaters are available only if the proper model names are assigned. You may need to restart the ArcFM Properties Manager after assigning model names to see all available autoupdaters.
- On the Model Names tab, assign class model names (Table 4 of worksheet).
- On the Field Model Names tab, assign field model names (Table 5 of worksheet).
- On the Object Info tab, assign object autoupdaters (Table 6 of worksheet).
- On the Field Display tab, set the order of the fields and the display properties for the feature.
-
Assign autoupdaters to the relationship classes (Table
3 of worksheet).
Examples
The instructions in this topic include an example. The example involves adding an air blown fiber feature to a fiber dataset that already has a geometric network.
A. Assign Class Model Names
On the Model Names tab in the ArcFM Properties Manager, assign the class model names from Table 4 of the worksheet. Below is a sample worksheet for class model names.
B. Assign Field Model Names and Autoupdaters
On the Field Model Names tab in the ArcFM Properties Manager, assign the field model names from Table 5 of the worksheet. Use the Field Info tab to assign any field autoupdaters. Below is a sample worksheet for field model names. The sample worksheet below does not contain ALL field model names. This is just a sample.
C. Assign Object Autoupdaters
On the Object Info tab in the ArcFM Properties Manager, assign the autoupdaters from Table 6 of the worksheet. Below is a sample worksheet for class autoupdaters.
D. Set Display Field
On the Field Display tab of the ArcFM Properties Manager, set the display field for the feature. This is the data displayed when a feature of this type is displayed in the Attribute Editor.
E. Assign Relationship Autoupdaters
Select the relationship class and open the ArcFM Properties Manager to assign autoupdaters. Below is a sample worksheet for relationships and their autoupdaters.