Abandon Settings

Use the Abandon Info tab to determine what happens to a feature when it is abandoned. You can select a class to which it is abandoned or abandoned and removed. You can also select an action to occur when a feature is abandoned.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?