Upgrade ArcFM Solution Database
The Upgrade ArcFM Solution Database tool updates your geodatabase
with modifications required by the latest release. The tool’s
button remains enabled on the ArcFM Solution
toolbar in ArcCatalog. You will only receive updates for the the ArcFM
applications that you have installed. If you do not have a particular
application installed (e.g., Designer), you will not receive any modifications
for it. You must be signed in as the data owner of the business tables
to upgrade the database. This tool also requires that there be a single
owner for all GIS tables in the geodatabase. The updates performed
are described on the "What's New" pages corresponding to each release.
Database version numbering
As of 10.0.3, database version numbers are no longer based on build numbers. The database version number is now based on the release number instead. When you upgrade your database, its version number is the ArcFM Solution release number.
Do not be alarmed by this message. The database version "1" corresponds with database version "10.0.3" or later.