Add to Existing Domain

  1. Right-click the geodatabase and select Properties.
  2. Select the Domains tab.
  3. Select the domain and add the model names to the Coded Values window.
  4. Click OK to save changes and close the Properties window.
    NOTE: If you cannot add a coded value or domain because there are no blank fields at the bottom of the window, check that the geodatabase is closed. You cannot add domains or model names to a geodatabase that is in use.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?