ArcCatalog Tools

This section covers the different ArcFM tools in ArcCatalog for helping you to configure your geodatabase. Each tool must be properly licensed and installed for it to be available. Contact Schneider Electric for licensing information.

NOTE: If you connect to the database (in ArcCatalog) using SQLExpress or a Personal ArcSDE connection, ArcFM tools will not be available. You must create a direct connect to the database in order to access ArcFM tools.
IMPORTANT: If you are running Windows Server 2012, you will need to run ArcCatalog as an administrator to get all ArcFM features.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?