Enable the Split On Edit

  1. Right-click a point feature and select the ArcFM Properties Manager.
  2. On the Object Info tab, set the Split on Edit property to Yes.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?