Enumerated Data Types

DHFC uses specific enumerations for some of the attribute fields. These enumerated data types are defined by the application and inform certain functionality. For that reason, they can only use the values declared, and they cannot be edited at your company site. However, you are able to map the same enumerated data type values to a domain defined by your GIS.

IMPORTANT: Do not change the coded domain values in your GIS once they have been put into production or have designs associated with them. If you change the coded values post-implementation, you inherently orphan data and the application fails to load.

Required

Feature Class/Object Table

Field Name

Enumeration

Description

RFCoupler and RFCoupler_D

CouplerType

0

TwoWay

1

ThreeWay

2

DirectionalCoupler

3

ThreeWayUnbalanced

Any that have the Workflow_Status field

Workflow_Status

0

AsBuilt

1

Proposed

UndergroundJunction and UndergroundJunction_D

UndergroundJunctionType

0

SharpTurn

1

BoreHole

Optional

Feature Class/Object Table

Field Name

Enumeration

Description

Any with an OH/UG Demarcation

RFOverheadUnderground

0

OH

1

UG

RFNode/RFNode_D

SegmentationMode

0

Non Segmented

2

Two Way

3

Three Way

4

Four Way

RFSplice/RFSplice_D

SpliceType

0

PBA

1

Straight

2

Block

3

Demarcation

RFTap/RFTap_D

ConditioningPluginType

20

CE

21

CS

22

RA

23

HT

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?