GIS Domain to Support Plugins
Conditioning taps and inline equalizers (LEQ/RC) can be coupled with a variety of plugins such as attenuators, cable equalizers, cable simulators, high tap values, and return path attenuators. If your company wants to use these plugin components, you need to add a domain to your GIS as described below. You do not have to add this domain if you do not intend on using components with plugins.
Create the domain while signed in as the ARCFM user.
-
Domain Name: RFConditioningPluginTypes
-
Field Type: Short Integer
-
Domain Type: Coded Value
-
Split Policy: Default Value
-
Merge Policy: Default Value
-
Coded Values:
The codes 20, 21, 22, and 23 correspond with the matching entry from the ComponentModelEnum in the Enumerated Data Types. The purpose of this domain is to identify what type of plugin a conditioning tap is using. The 0 entry is what appears when no plugin is selected in a tap. The 99 entry is used to indicate that the plugin is a jumper.