Security Considerations
This topic provides security considerations for ArcGIS configuration, in addition to security recommendations that are relatively standard across all XI series apps.
ArcGIS Server Considerations
-
All ArcGIS Servers must be protected against cross-site scripting attacks by configuring the origins allowed to be accessed alongside content from ArcGIS Server.
IMPORTANT: It is crucial that you follow the instructions to Restrict cross-domain requests to ArcGIS Server and also secure your ArcGIS Server site according to the guidelines that Esri provides. -
ArcGIS Server is usually hosted within another HTTP stack (IIS, Apache). Follow the vendor's best practices for hardening the server against attack.
-
If you install ArcGIS Web Adaptor to allow ArcGIS Server to integrate with your existing web server, you must enable HTTPS on your web server, which means you need to obtain a server certificate and bind it to the website that hosts ArcGIS Web Adaptor.
-
You must specify the log retention period for ArcGIS Server logs. The retention period aligns with your policy but we recommend the debug level be set to the default value of Error. Only change this setting when actively troubleshooting an issue. The ArcGIS Server logs should never be disabled. See the Esri topic about how to specify server log settings for more information.
Portal for ArcGIS Considerations
-
Your Portal-based authentication can use Portal built-in users or Active Directory (AD)-based users.
-
Whether you use built-in users or AD-based users, you need to let traffic come from Auth0 (a hosted service that enables single sign-on) through the firewall to your Portal instance.
-
Decide which groups, whether built-in or AD-based, map to which roles as specified in the ArcFM Solution XI Series Named User Functionality Matrix. We make assignments via group information from the identity provider so that group membership can be managed in a central location.
-
Refer to Esri’s recommendations for securing your portal, which are outlined in their securing your portal article.
Client Devices that Run the DHFC XI Application
DHFC provides users with access to an important asset of the organization: its GIS data. As such, it is important to secure that data against theft.
For Windows, refer to Microsoft's documentation on BitLocker.
Recommendations specifically for securing client devices:
-
Enable full disk encryption on devices that host Solution Center.
-
Configure screen lock timeout for a maximum of five minutes.
-
For Windows specific settings:
-
Do not grant local administrator privileges to end users.
-
Do not grant end-user account permissions to install applications.
-
Use application “allow-listing” to permit only approved applications or executables to run.
-
Use real-time endpoint protection to detect unauthorized changes to installed components.
-
Schneider Electric recommends you give users access only to secure locations determined by your IT department. File permissions are managed by the user’s Windows profile.
-
Abandoned File Directories After Upgrading from Squirrel to MSIX
As described in the myArcFM article Designer HFC MSIX Migration, the application uses MSIX installer technology, and it no longer uses the previous Squirrel installer technology.
After you upgrade using the MSIX installer, some file directories from the Squirrel installer are left behind. These include the following:
-
%appdata%\local\CoaxNetworkDesigner: This is where the client application settings were stored. Once you have upgraded, these settings are no longer used, and you can safely delete this directory.
-
%appdata%\roaming\SE.Coax.NetworkDesigner: This is where the logs were stored when using the Squirrel installer. You might want to keep the logs for historical purposes. You can either leave them in the directory, or you can copy them to another location. If you copy them to a different location, you can then safely delete this directory.
-
%appdata%\local\Schneider_Electric\DesignerHFC*: This is where dialog location settings were stored. You might have multiple child folders depending on how many versions you have installed using the Squirrel installer. Once you have upgraded, these settings are no longer used, and you can safely delete this directory.
Uninstalling the Application and Transferring Equipment:
Uninstall the application from either:
-
The Apps & features menu on your computer. Locate the application, then click Uninstall.
-
The Start Menu on your computer. Right-click the application icon, then choose Uninstall.
After uninstalling the application, the following files and directories are still present.
-
Logs stored in C:\ProgramData\Schneider Electric\SE.Coax.NetworkDesigner.
-
Settings stored in C:\ProgramData\Packages\ArcFMDHFC_qybjwhg5w8jy8. If this directory is not deleted and the user reinstalls, any Settings changes previously made are restored.
If your company intends to transfer the equipment to another user, you should follow best practices for the secured deletion of these directories.
Privacy Policy
For details about how Schneider Electric processes and protects your personal information, refer to the ArcFM Privacy article on myArcFM.
Digital Signatures
Schneider Electric ArcFM XI series software is always digitally signed. However, in the extremely rare event that an issue arises, the software should not be installed and you should contact Technical Support. If the application doesn’t open, then there might be an issue with the validity of the digital signature.
For an extra level of security, you can manually check the digital signature for any of our software. You have a couple options:
Digital Signature Details
-
Contact Technical Support to obtain the digitally-signed hash number for the executable that we deployed to you.
-
Right-click the executable and select Properties > Digital Signatures tab.
-
Under Signature List, select the Schneider Electric entry and click Details. You can view the signing status near the top of the Digital Signatures Details window.
-
Under Countersignatures, select DigiCert Timestamp and click Details.
-
In the Signature section, look for Subject Key Identifier and select it.
-
Using the hash number in the Value section, compare it with the one Technical Support provided.
-
If they don’t match, you should contact Technical Support to obtain the properly signed executable.
Command Line Hash Comparison
-
Contact Technical Support to obtain the digitally-signed hash number for the executable that we deployed to you.
-
At a command prompt, switch to the subfolder where the executable is located.
-
Type
Get-FileHash <name of executable>.exe | Format-List
and hit Enter, after which you are given a hash number. -
At the command prompt, type
(Get-FileHash <name of executable>.exe).hash -eq “<hash number given to you by Technical Support>”
and hit Enter. You then receive a response of True or False. -
If the response is false, you should contact Technical Support to obtain the properly signed executable.