Required Fields for All Feature Classes

All feature classes require the following:

Field Name

Data Type

Notes

NetworkID

GUID

Unique identifier for the component or record.

ObjectID

Object ID

Esri Object Id for the feature or object.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?