In-Design Dataset (Coax_D) and As-Built Dataset (Fiber)
As stated in the High-Level Architecture of the Geodatabase topic, there are two identical copies of these feature classes. One has the suffix “_D” to indicate its in-design state, the other does not have the suffix to indicate its as-built state.
Because all the fields are identical, each feature class is listed only once in these topics. However, in your implementation, the feature class is present in the geodatabase twice, using the naming convention mentioned above.
RFAmplifier
<Table CoaxName="RFAmplifierData" EsriDesignName="RFAmplifier_D" EsriBuiltName="RFAmplifier">
This is a point feature class with the following required fields:
|
Field Name |
Data Type |
Notes |
|---|---|---|
|
NetworkID |
GUID |
Unique identifier for the component or record. |
|
ObjectID |
Object ID |
Esri Object Id for the feature or object. |
|
AerialStructureId |
GUID |
NetworkId of the overhead structure that this component is associated with; an empty GUID means this component is not associated with any overhead structure. |
|
AmpNumber |
Long Integer |
The unique number of the amplifier within the node (0–99). |
|
CatalogId |
String |
The Id of the DHFC catalog spec associated with the component; should be a string representation of a valid GUID in the following format, 6A1F97AD-C665-4521-B954-29A4429FC128. |
|
FedFromComponentId |
GUID |
The NetworkId of the upstream component providing RF signal to the component. |
|
Flipped |
Short Integer |
Boolean (typically Yes/No) indicating whether the component is flipped from its default position. |
|
ForwardEqId |
String |
The component’s NetworkId formatted as {92DB7597-AEC3-459E-A10A-A05235D1E85E}:Forward. |
|
ForwardPadId |
String |
The component’s NetworkId formatted as {92DB7597-AEC3-459E-A10A-A05235D1E85E}:Forward. |
|
HotDotPortNumber |
Long Integer |
The number of the port with the lowest signal loss. |
|
InternalCouplerCompanyID1 |
String |
The ID of the spec that is connected to plugin slot #1 of the amplifier. Schneider Electric recommends a default value of null.. |
|
InternalCouplerCompanyID2 |
String |
The ID of the spec that is connected to plugin slot #2 of the amplifier. Schneider Electric recommends a default value of null.. |
|
InternalCouplerCompanyID3 |
String |
The ID of the spec that is connected to plugin slot #3 of the amplifier. Schneider Electric recommends a default value of null.. |
|
InternalCouplerValue1 |
String |
A value describing the internal coupler used in the forward output profile of the amplifier. When a splitter is used as the internal coupler, the value is the port count. When a directional coupler is used as the internal coupler, the value is the tap value of the directional coupler. This field maps to the forward output frequency profile #1. |
|
InternalCouplerValue2 |
String |
A value describing the internal coupler used in the forward output profile of the amplifier. When a splitter is used as the internal coupler, the value is the port count. When a directional coupler is used as the internal coupler, the value is the tap value of the directional coupler. This field maps to the forward output frequency profile #2. |
|
InternalCouplerValue3 |
String |
A value describing the internal coupler used in the forward output profile of the amplifier. When a splitter is used as the internal coupler, the value is the port count. When a directional coupler is used as the internal coupler, the value is the tap value of the directional coupler. This field maps to the forward output frequency profile #3. |
|
InternalPowerMapping |
String |
Generated by the application in the format: |
|
IsInMDU |
Short Integer |
Boolean (typically Yes/No) indicating whether or not the component is found within an Multi-Dwelling Unit (MDU). |
|
IsLocked |
Short Integer |
Boolean (typically Yes/No) indicating whether the component is locked in DHFC; locked components cannot be edited and are excluded from DHFC's auto-optimization feature. |
|
ModelNumber |
String |
The component model number. |
|
Name |
String |
The component name. |
|
NodeId |
GUID |
The NetworkID of the component’s node. |
|
PortConfiguraiton |
String |
Generated by the application; list of ports with active legs: A B C D E F. |
|
PoweringFedFromComponentId |
GUID |
The NetworkId of the component which supplies power to the this component. |
|
ReturnEqId |
String |
The component’s NetworkId formatted as {92DB7597-AEC3-459E-A10A-A05235D1E85E}:Return. |
|
ReturnPadId |
String |
The component’s NetworkId formatted as {92DB7597-AEC3-459E-A10A-A05235D1E85E}:Return. |
|
SymbolRotation |
Double |
The component’s symbol rotation. |
|
UGStructureId |
GUID |
The NetworkId of the underground structure that this component is associated with; an empty GUID means this component is not associated with any underground structure. |
|
Workflow_Status |
String |
WorkflowState enumeration: AsBuilt and Proposed; for more information, refer to the topic Enumerated Data Types. |
RFCable
<Table CoaxName="RFCableData" EsriDesignName="RFCable_D" EsriBuiltName="RFCable">
This is a line feature class with the following required fields:
|
Field Name |
Data Type |
Notes |
|---|---|---|
|
NetworkID |
GUID |
Unique identifier for the component or record. |
|
ObjectID |
Object ID |
Esri Object Id for the feature or object. |
|
CatalogId |
String |
The Id of the DHFC catalog spec associated with the component; should be a string representation of a valid GUID in the following format, 6A1F97AD-C665-4521-B954-29A4429FC128. |
|
FedFromComponentId |
GUID |
The NetworkId of the upstream component providing RF signal to the component. |
|
IsInMDU |
Short Integer |
Boolean (typically Yes/No) indicating whether or not the component is found within an Multi-Dwelling Unit (MDU). |
|
IsLocked |
Short Integer |
Boolean (typically Yes/No) indicating whether the component is locked in DHFC; locked components cannot be edited and are excluded from DHFC's auto-optimization feature. |
|
Length |
Double |
The length of the cable; this value is automatically provided by DHFC based on the strand length, but it can be overridden by the user |
|
ModelNumber |
String |
The component model number. |
|
PoweringFedFromComponentId |
GUID |
The NetworkId of the component which supplies power to the this component. |
|
Workflow_Status |
String |
WorkflowState enumeration: AsBuilt and Proposed; for more information, refer to the topic Enumerated Data Types. |
RFCoupler
<Table CoaxName="RFCouplerData" EsriDesignName="RFCoupler_D" EsriBuiltName="RFCoupler">
This is a point feature class with the following required fields:
|
Field Name |
Data Type |
Notes |
|---|---|---|
|
NetworkID |
GUID |
Unique identifier for the component or record. |
|
ObjectID |
Object ID |
Esri Object Id for the feature or object. |
|
AerialStructureId |
GUID |
NetworkId of the overhead structure that this component is associated with; an empty GUID means this component is not associated with any overhead structure. |
|
CatalogId |
String |
The Id of the DHFC catalog spec associated with the component; should be a string representation of a valid GUID in the following format, 6A1F97AD-C665-4521-B954-29A4429FC128. |
|
CouplerType |
Short Integer |
CouplerType enumeration: TwoWay, ThreeWay, DirectionalCoupler, ThreeWayUnbalanced. For more information, see Enumerated Data Types. |
|
FedFromComponentId |
GUID |
The NetworkId of the upstream component providing RF signal to the component. |
|
Flipped |
Short Integer |
Boolean (typically Yes/No) indicating whether the component is flipped from its default position. |
|
HotDotPortNumber |
Long Integer |
The number of the port with the lowest signal loss. |
|
InternalPowerMapping |
String |
Generated by the application in the format: |
|
IsInMDU |
Short Integer |
Boolean (typically Yes/No) indicating whether or not the component is found within an Multi-Dwelling Unit (MDU). |
|
IsLocked |
Short Integer |
Boolean (typically Yes/No) indicating whether the component is locked in DHFC; locked components cannot be edited and are excluded from DHFC's auto-optimization feature. |
|
ModelNumber |
String |
The component model number. |
|
PortCount |
Short Integer |
The number of output ports on the component |
|
PoweringFedFromComponentId |
GUID |
The NetworkId of the component which supplies power to the this component. |
|
SymbolRotation |
Double |
The component’s symbol rotation. |
|
UGStructureId |
GUID |
The NetworkId of the underground structure that this component is associated with; an empty GUID means this component is not associated with any underground structure. |
|
Workflow_Status |
String |
WorkflowState enumeration: AsBuilt and Proposed; for more information, refer to the topic Enumerated Data Types. |
RFDoNotBuildBoundary
<Table CoaxName="RFDoNotBuildBoundaryData" EsriDesignName="RFDoNotBuildBoundary_D" EsriBuiltName="RFDoNotBuildBoundary">
This is a polygon feature class with the following required fields:
|
Field Name |
Data Type |
Notes |
|---|---|---|
|
NetworkID |
GUID |
Unique identifier for the component or record. |
|
ObjectID |
Object ID |
Esri Object Id for the feature or object. |
|
IsInMDU |
Short Integer |
Boolean (typically Yes/No) indicating whether or not the component is found within an Multi-Dwelling Unit (MDU). |
|
Name |
String |
The component name. |
|
NetworkChangeNumber |
String |
The network change number |
RFHotDot
<Table CoaxName="RFHotDotData" EsriDesignName="RFHotDot_D" EsriBuiltName="RFHotDot">
This is a point feature class with the following required fields:
|
Field Name |
Data Type |
Notes |
|---|---|---|
|
NetworkID |
GUID |
Unique identifier for the component or record. |
|
ObjectID |
Object ID |
Esri Object Id for the feature or object. |
|
IsInMDU |
Short Integer |
Boolean (typically Yes/No) indicating whether or not the component is found within an Multi-Dwelling Unit (MDU). |
|
SymbolRotation |
Double |
The component’s symbol rotation. |
RFHousingToHousing
<Table CoaxName="RFHousingToHousingData" EsriDesignName="RFHousingToHousing_D" EsriBuiltName="RFHousingToHousing">
This is a line feature class with the following required fields:
|
Field Name |
Data Type |
Notes |
|---|---|---|
|
NetworkID |
GUID |
Unique identifier for the component or record. |
|
ObjectID |
Object ID |
Esri Object Id for the feature or object. |
|
AerialStructureId |
GUID |
NetworkId of the overhead structure that this component is associated with; an empty GUID means this component is not associated with any overhead structure. |
|
Angle |
Double |
The angle of the point geometry for the component |
|
CatalogId |
String |
The Id of the DHFC catalog spec associated with the component; should be a string representation of a valid GUID in the following format, 6A1F97AD-C665-4521-B954-29A4429FC128. |
|
FedFromComponentId |
GUID |
The NetworkId of the upstream component providing RF signal to the component. |
|
Flipped |
Short Integer |
Boolean (typically Yes/No) indicating whether the component is flipped from its default position. |
|
IsInMDU |
Short Integer |
Boolean (typically Yes/No) indicating whether or not the component is found within an Multi-Dwelling Unit (MDU). |
|
IsLocked |
Short Integer |
Boolean (typically Yes/No) indicating whether the component is locked in DHFC; locked components cannot be edited and are excluded from DHFC's auto-optimization feature. |
|
LocationX |
Double |
The component’s X location |
|
LocationY |
Double |
The component’s Y location |
|
ModelNumber |
String |
The component model number. |
|
PoweringFedFromComponentId |
GUID |
The NetworkId of the component which supplies power to the this component. |
|
UGStructureId |
GUID |
The NetworkId of the underground structure that this component is associated with; an empty GUID means this component is not associated with any underground structure. |
|
Workflow_Status |
String |
WorkflowState enumeration: AsBuilt and Proposed; for more information, refer to the topic Enumerated Data Types. |
RFInlineEq
<Table CoaxName="RFInlineEqData" EsriDesignName="RFInlineEq_D" EsriBuiltName="RFInlineEq">
This is a point feature class with the following required fields:
|
Field Name |
Data Type |
Notes |
|---|---|---|
|
NetworkID |
GUID |
Unique identifier for the component or record. |
|
ObjectID |
Object ID |
Esri Object Id for the feature or object. |
|
AerialStructureId |
GUID |
NetworkId of the overhead structure that this component is associated with; an empty GUID means this component is not associated with any overhead structure. |
|
CatalogId |
String |
The Id of the DHFC catalog spec associated with the component; should be a string representation of a valid GUID in the following format, 6A1F97AD-C665-4521-B954-29A4429FC128. |
|
ConditioningPluginCID |
GUID |
This is the catalog ID of the plugin spec used in an inline equalizer (LEQ/RC). This field is required only if your company is using plugins. If you are not using plugins, this field is optional. |
|
ConditioningPluginModelNumber |
String, 50 length |
This is the model number of the plugin spec used in an inline equalizer (LEQ/RC). This field is required only if your company is using plugins. If you are not using plugins, this field is optional. |
|
ConditioningPluginValue |
Double |
This is the PadValue from the return attenuator plugin spec in the catalog. This value is only sent to GIS and is ignored on import. This field is required only if your company is using plugins. If you are not using plugins, this field is optional. |
|
FedFromComponentId |
GUID |
The NetworkId of the upstream component providing RF signal to the component. |
|
Flipped |
Short Integer |
Boolean (typically Yes/No) indicating whether the component is flipped from its default position. |
|
InternalPoweringMapping |
String |
Generated by the application in the format: |
|
IsInMDU |
Short Integer |
Boolean (typically Yes/No) indicating whether or not the component is found within an Multi-Dwelling Unit (MDU). |
|
IsLocked |
Short Integer |
Boolean (typically Yes/No) indicating whether the component is locked in DHFC; locked components cannot be edited and are excluded from DHFC's auto-optimization feature. |
|
ModelNumber |
String |
The component model number. |
|
PoweringFedFromComponentId |
GUID |
The NetworkId of the component which supplies power to the this component. |
|
SymbolRotation |
Double |
The component’s symbol rotation. |
|
UGStructureId |
GUID |
The NetworkId of the underground structure that this component is associated with; an empty GUID means this component is not associated with any underground structure. |
|
Workflow_Status |
String |
WorkflowState enumeration: AsBuilt and Proposed; for more information, refer to the topic Enumerated Data Types. |
RFNode
<Table CoaxName="RFNodeData" EsriDesignName="RFNode_D" EsriBuiltName="RFNode">
This is a point feature class with the following required fields:
|
Field Name |
Data Type |
Notes |
|---|---|---|
|
NetworkID |
GUID |
Unique identifier for the component or record. |
|
ObjectID |
Object ID |
Esri Object Id for the feature or object. |
|
AerialStructureId |
GUID |
NetworkId of the overhead structure that this component is associated with; an empty GUID means this component is not associated with any overhead structure. |
|
CatalogId |
String |
The Id of the DHFC catalog spec associated with the component; should be a string representation of a valid GUID in the following format, 6A1F97AD-C665-4521-B954-29A4429FC128. |
|
FedFromComponentId |
GUID |
The NetworkId of the upstream component providing RF signal to the component. |
|
Flipped |
Short Integer |
Boolean (typically Yes/No) indicating whether the component is flipped from its default position. |
|
InternalPowerMapping |
String |
Generated by the application in the format: |
|
IsInMDU |
Short Integer |
Boolean (typically Yes/No) indicating whether or not the component is found within an Multi-Dwelling Unit (MDU). |
|
IsLocked |
Short Integer |
Boolean (typically Yes/No) indicating whether the component is locked in DHFC; locked components cannot be edited and are excluded from DHFC's auto-optimization feature. |
|
ModelNumber |
String |
The component model number. |
|
Name |
String |
The component name. |
|
PortConfiguration |
String |
Generated by the application; list of ports with active legs: A B C D E F. See the topic RFNode and the PortConfiguration Field for more information. |
|
PoweringFedFromComponentId |
GUID |
The NetworkId of the component which supplies power to the this component. |
|
PowerSupplyId |
GUID |
The NetworkId of the power supply that powers this component |
|
ProjectFileCatalogId |
GUID |
The GUID of the project file used to create the node; this value corresponds to the DHFC catalog’s ProjectFile.Id column. The field is populated when a node is pushed to the GIS. IMPORTANT: If the application encounters a null ProjectFileCatalogId
(for example, if opening an older design prior to upgrading to 11.4
and beyond), the application falls back to locating the project file
by name. This means, if both the ProjectFileCatalogId is null and the project file name has been changed, the older design cannot
be loaded. Thus, during your transition to version 11.4 and beyond,
do not change any project file names until after older designs are
pushed or otherwise cleared from the system.
|
|
ProjectFileName |
String |
The name of the project file used to create the node; this value corresponds to the DHFC catalog’s ProjectFile.Name column |
|
SegmentationConfiguration |
String |
This field is required if your company uses segmentable nodes. Otherwise, it is optional. When a node is segmented, the SegmentationConfiguration field contains information about the nodes and the legs they serve. The length of this field should be the Node Name field length + 50. For example, if your Node Name field length is limited to 45, then this field’s length should be 95 (45 + 50). When a node is not segmented, this field is null. |
|
SegmentationMode |
Short Integer |
This field is required if your company uses segmentable nodes. Otherwise, it is optional. Segmentable nodes come in a handful of configurations, from non-segmented to four-way. This field is associated to the RF Node Segmentation Mode domain. |
|
SymbolRotation |
Double |
The component’s symbol rotation. |
|
UGStructureId |
GUID |
The NetworkId of the underground structure that this component is associated with; an empty GUID means this component is not associated with any underground structure. |
|
Workflow_Status |
String |
WorkflowState enumeration: AsBuilt and Proposed; for more information, refer to the topic Enumerated Data Types. |
RFNodeBoundary
<Table CoaxName="RFNodeBoundaryData" EsriDesignName="RFNodeBoundary_D" EsriBuiltName="RFNodeBoundary">
This is a polygon feature class with the following required fields:
|
Field Name |
Data Type |
Notes |
|---|---|---|
|
NetworkID |
GUID |
Unique identifier for the component or record. |
|
ObjectID |
Object ID |
Esri Object Id for the feature or object. |
|
Name |
String |
The node boundary name, which is typically the name of the node the boundary encompasses. This is a required field that cannot be null. |
|
NodeNetworkId |
GUID |
The NetworkId of the node the boundary is associated with. This field must be populated and cannot be an empty GUID. |
|
Workflow_Status |
String |
WorkflowState enumeration: AsBuilt and Proposed; for more information, refer to the topic Enumerated Data Types. |
RFPowerBlock
<Table CoaxName="RFPowerBlockData" EsriDesignName="RFPowerBlock_D" EsriBuiltName="RFPowerBlock">
This is a point feature class with the following required fields:
|
Field Name |
Data Type |
Notes |
|---|---|---|
|
NetworkID |
GUID |
Unique identifier for the component or record. |
|
ObjectID |
Object ID |
Esri Object Id for the feature or object. |
|
IsInMDU |
Short Integer |
Boolean (typically Yes/No) indicating whether or not the component is found within an Multi-Dwelling Unit (MDU). |
|
SymbolRotation |
Double |
The component’s symbol rotation. |
|
Workflow_Status |
String |
WorkflowState enumeration: AsBuilt and Proposed; for more information, refer to the topic Enumerated Data Types. |
RFPowerInserter
<Table CoaxName="RFPowerInserterData" EsriDesignName="RFPowerInserter_D" EsriBuiltName="RFPowerInserter">
This is a point feature class with the following required fields:
|
Field Name |
Data Type |
Notes |
|---|---|---|
|
NetworkID |
GUID |
Unique identifier for the component or record. |
|
ObjectID |
Object ID |
Esri Object Id for the feature or object. |
|
AerialStructureId |
GUID |
NetworkId of the overhead structure that this component is associated with; an empty GUID means this component is not associated with any overhead structure. |
|
CatalogId |
String |
The Id of the DHFC catalog spec associated with the component; should be a string representation of a valid GUID in the following format, 6A1F97AD-C665-4521-B954-29A4429FC128. |
|
FedFromComponentId |
GUID |
The NetworkId of the upstream component providing RF signal to the component. |
|
Flipped |
Short Integer |
Boolean (typically Yes/No) indicating whether the component is flipped from its default position. |
|
InternalPowerMapping |
String |
Generated by the application in the format: |
|
IsInMDU |
Short Integer |
Boolean (typically Yes/No) indicating whether or not the component is found within an Multi-Dwelling Unit (MDU). |
|
IsLocked |
Short Integer |
Boolean (typically Yes/No) indicating whether the component is locked in DHFC; locked components cannot be edited and are excluded from DHFC's auto-optimization feature. |
|
ModelNumber |
String |
The component model number. |
|
PoweringFedFromComponentId |
GUID |
The NetworkId of the component which supplies power to the this component. |
|
SymbolRotation |
Double |
The component’s symbol rotation. |
|
UGStructureId |
GUID |
The NetworkId of the underground structure that this component is associated with; an empty GUID means this component is not associated with any underground structure. |
|
Workflow_Status |
String |
WorkflowState enumeration: AsBuilt and Proposed; for more information, refer to the topic Enumerated Data Types. |
RFPowerSupply
<Table CoaxName="RFPowerSupplyData" EsriDesignName="RFPowerSupply_D" EsriBuiltName="RFPowerSupply">
This is a point feature class with the following required fields:
|
Field Name |
Data Type |
Notes |
|---|---|---|
|
NetworkID |
GUID |
Unique identifier for the component or record. |
|
ObjectID |
Object ID |
Esri Object Id for the feature or object. |
|
AerialStructureId |
GUID |
NetworkId of the overhead structure that this component is associated with; an empty GUID means this component is not associated with any overhead structure. |
|
CatalogId |
String |
The Id of the DHFC catalog spec associated with the component; should be a string representation of a valid GUID in the following format, 6A1F97AD-C665-4521-B954-29A4429FC128. |
|
FedFromComponentId |
GUID |
The NetworkId of the upstream component providing RF signal to the component. |
|
Flipped |
Short Integer |
Boolean (typically Yes/No) indicating whether the component is flipped from its default position. |
|
IsInMDU |
Short Integer |
Boolean (typically Yes/No) indicating whether or not the component is found within an Multi-Dwelling Unit (MDU). |
|
IsLocked |
Short Integer |
Boolean (typically Yes/No) indicating whether the component is locked in DHFC; locked components cannot be edited and are excluded from DHFC's auto-optimization feature. |
|
ModelNumber |
String |
The component model number. |
|
Name |
String |
The component name. |
|
PoweringFedFromComponentId |
GUID |
The NetworkId of the component which supplies power to the this component. This is not a required field as of version 11.4.1. The power supply is the top level object in the power network, so nothing feeds it. |
|
SymbolRotation |
Double |
The component’s symbol rotation. |
|
UGStructureId |
GUID |
The NetworkId of the underground structure that this component is associated with; an empty GUID means this component is not associated with any underground structure. |
|
Workflow_Status |
String |
WorkflowState enumeration: AsBuilt and Proposed; for more information, refer to the topic Enumerated Data Types. |
RFPowerSupplyBoundary
<Table CoaxName="RFPowerSupplyBoundaryData" EsriDesignName="RFPowerSupplyBoundary_D" EsriBuiltName="RFPowerSupplyBoundary">
This is a polygon feature class with the following required fields:
|
Field Name |
Data Type |
Notes |
|---|---|---|
|
NetworkID |
GUID |
Unique identifier for the component or record. |
|
ObjectID |
Object ID |
Esri Object Id for the feature or object. |
|
Name |
String |
The component name. |
|
Workflow_Status |
String |
WorkflowState enumeration: AsBuilt and Proposed; for more information, refer to the topic Enumerated Data Types. |
RFSegmentableNodeBoundary
<Table CoaxName="RFSegmentableNodeBoundaryData" EsriDesignName="RFSegmentableNodeBoundary_D" EsriBuiltName="RFSegmentableNodeBoundary">
This is a polygon feature class with the following required fields:
|
Field Name |
Data Type |
Notes |
|---|---|---|
|
NetworkID |
GUID |
Unique identifier for the component or record. |
|
ObjectID |
Object ID |
Esri Object Id for the feature or object. |
|
Hubsite |
String |
Allows the utility to track the hubsite name for the service area. |
|
LegsServed |
String |
Keeps track of which legs are served within the segmentable node boundary. |
|
LegsServedLabels |
String |
Preserves the list of labels for the legs served in each segmentable node boundary. |
|
Market |
String |
Allows the utility to track the market name for the service area. |
|
Name |
String |
The segmentable node boundary name, which is typically the name of the node the boundary encompasses. This is a required field that cannot be null. See the Using Guide topic Configure Segmentation and Assign Legs for more details about how the leg names affect the node name. |
|
NodeNetworkId |
GUID |
The NetworkId of the node the boundary is associated with. This field must be populated and cannot be an empty GUID. |
|
Workflow_Status |
String |
WorkflowState enumeration: AsBuilt and Proposed; for more information, refer to the topic Enumerated Data Types. |
RFSplice
<Table CoaxName="RFSpliceData" EsriDesignName="RFSplice_D" EsriBuiltName="RFSplice">
This is a point feature class with the following required fields:
|
Field Name |
Data Type |
Notes |
|---|---|---|
|
NetworkID |
GUID |
Unique identifier for the component or record. |
|
ObjectID |
Object ID |
Esri Object Id for the feature or object. |
|
AerialStructureId |
GUID |
NetworkId of the overhead structure that this component is associated with; an empty GUID means this component is not associated with any overhead structure. |
|
CatalogId |
String |
The Id of the DHFC catalog spec associated with the component; should be a string representation of a valid GUID in the following format, 6A1F97AD-C665-4521-B954-29A4429FC128. |
|
FedFromComponentId |
GUID |
The NetworkId of the upstream component providing RF signal to the component. |
|
FeedsComponentID |
GUID |
NetworkId of the component that is connected to the “downstream” side of the splice |
|
IsInMDU |
Short Integer |
Boolean (typically Yes/No) indicating whether or not the component is found within an Multi-Dwelling Unit (MDU). |
|
IsLocked |
Short Integer |
Boolean (typically Yes/No) indicating whether the component is locked in DHFC; locked components cannot be edited and are excluded from DHFC's auto-optimization feature. |
|
ModelNumber |
String |
The component model number. |
|
PoweringFedFromComponentId |
GUID |
The NetworkId of the component which supplies power to the this component. |
|
SymbolRotation |
Double |
The component’s symbol rotation. |
|
UGStructureId |
GUID |
The NetworkId of the underground structure that this component is associated with; an empty GUID means this component is not associated with any underground structure. |
|
Workflow_Status |
String |
WorkflowState enumeration: AsBuilt and Proposed; for more information, refer to the topic Enumerated Data Types. |
RFTap
<Table CoaxName="RFTapData" EsriDesignName="RFTap_D" EsriBuiltName="RFTap">
This is a point feature class with the following required fields:
|
Field Name |
Data Type |
Notes |
|---|---|---|
|
NetworkID |
GUID |
Unique identifier for the component or record. |
|
ObjectID |
Object ID |
Esri Object Id for the feature or object. |
|
AerialStructureId |
GUID |
NetworkId of the overhead structure that this component is associated with; an empty GUID means this component is not associated with any overhead structure. |
|
CatalogId |
String |
The Id of the DHFC catalog spec associated with the component; should be a string representation of a valid GUID in the following format, 6A1F97AD-C665-4521-B954-29A4429FC128. |
|
ConditioningPluginCID |
GUID |
This is the catalog ID of the plugin spec used in a conditioning tap. This field is required only if your company is using plugins. If you are not using plugins, this field is optional. |
|
ConditioningPluginModelNumber |
String, 50 length |
This is the model number of the plugin spec used in a conditioning tap. This field is required only if your company is using plugins. If you are not using plugins, this field is optional. |
|
ConditioningPluginType |
Short Integer |
This is the type of plugin that is used in a tap. This field must use the RFConditioningPluginTypes domain. This field is required only if your company is using plugins. If you are not using plugins, this field is optional. |
|
ConditioningPluginValue |
Double |
This is the value of how much the plugin affects the signal. For CE, CS and HT plugins, this is the EqualizerValue from the plugin spec in the catalog. For RA/pads, this is the PadValue from the plugin spec in the catalog. This value is only sent to GIS and ignored on import. This field is required only if your company is using plugins. If you are not using plugins, this field is optional. |
|
FedFromComponentId |
GUID |
The NetworkId of the upstream component providing RF signal to the component. |
|
Flipped |
Short Integer |
Boolean (typically Yes/No) indicating whether the component is flipped from its default position. |
|
IsInMDU |
Short Integer |
Boolean (typically Yes/No) indicating whether or not the component is found within an Multi-Dwelling Unit (MDU). |
|
IsLocked |
Short Integer |
Boolean (typically Yes/No) indicating whether the component is locked in DHFC; locked components cannot be edited and are excluded from DHFC's auto-optimization feature. |
|
ModelNumber |
String |
The component model number. |
|
Name |
String |
The component name. The default value can be null. |
|
PortCount |
Short Integer |
Count of ports. |
|
PoweringFedFromComponentId |
GUID |
The NetworkId of the component which supplies power to the this component. |
|
SymbolRotation |
Double |
The component’s symbol rotation. |
|
UGStructureId |
GUID |
The NetworkId of the underground structure that this component is associated with; an empty GUID means this component is not associated with any underground structure. |
|
Workflow_Status |
String |
WorkflowState enumeration: AsBuilt and Proposed; for more information, refer to the topic Enumerated Data Types. |
RFTerminator
<Table CoaxName="RFTerminatorData" EsriDesignName="RFTerminator_D" EsriBuiltName="RFTerminator">
This is a point feature class with the following required fields:
|
Field Name |
Data Type |
Notes |
|---|---|---|
|
NetworkID |
GUID |
Unique identifier for the component or record. |
|
ObjectID |
Object ID |
Esri Object Id for the feature or object. |
|
AerialStructureId |
GUID |
NetworkID of the overhead structure associated with the component; an empty GUID means the component is not associated with any overhead structure |
|
CatalogId |
String |
The Id of the DHFC catalog spec associated with the component; should be a string representation of a valid GUID in the following format, 6A1F97AD-C665-4521-B954-29A4429FC128. |
|
FedFromComponentId |
GUID |
The NetworkId of the upstream component providing RF signal to the component. |
|
IsInputTerminator |
Short Integer |
Boolean (typically Yes/No) indicating whether or not the component terminates RF input |
|
IsInMDU |
Short Integer |
Boolean (typically Yes/No) indicating whether or not the component is found within an Multi-Dwelling Unit (MDU). |
|
IsLocked |
Short Integer |
Boolean (typically Yes/No) indicating whether the component is locked in DHFC; locked components cannot be edited and are excluded from DHFC's auto-optimization feature. |
|
ModelNumber |
String |
The component model number. |
|
Name |
String |
The component name. |
|
PoweringFedFromComponentId |
GUID |
The NetworkId of the component which supplies power to the this component. |
|
SymbolRotation |
Double |
The component’s symbol rotation. |
|
UGStructureId |
GUID |
The NetworkId of the underground structure that this component is associated with; an empty GUID means this component is not associated with any underground structure. |
|
Workflow_Status |
String |
WorkflowState enumeration: AsBuilt and Proposed; for more information, refer to the topic Enumerated Data Types. |