RFNode_RFNodeCoaxPort
There are two versions of this relationship:
-
RFNode_RFNodeCoaxPort for the as-built representation.
-
RFNode_RFNodeCoaxPort_D for the in-design representation.
For step-by-step instructions, read the topic RFCoupler_RFCouplerPort. Because the steps are the same, only the relevant properties are included in this topic.
RFNode_RFNodeCoaxPort, the As-Built Relationship
|
Relationship Class Property |
Value or Choice |
|---|---|
|
Name |
RFNode_RFNodeCoaxPort |
|
Origin Table or Feature Class |
RFNode |
|
Destination Table or Feature Class |
RFNodeCoaxPort |
|
Relationship Type |
Simple |
|
Forward Label |
RFNodeCoaxPort
IMPORTANT: The Forward Label you
type while creating the relationship must match the EsriBuiltName
entry in the Schema.xml file for this component.
|
|
Backward Label |
RFNode |
|
Message Direction |
None (no messages propagated) |
|
Cardinality |
1–M (one to many) |
|
Relationship Attributes |
No, I do not want to add attributes to this relationship class |
|
Primary Key |
NetworkId |
|
Foreign Key |
NodeId |
RFNode_RFNodeCoaxPort_D, the In-Design Relationship
|
Relationship Class Property |
Value or Choice |
|---|---|
|
Name |
RFNode_RFNodeCoaxPort_D |
|
Origin Table or Feature Class |
RFNode_D |
|
Destination Table or Feature Class |
RFNodeCoaxPort_D |
|
Relationship Type |
Simple |
|
Forward Label |
SECom.ARCFM.RFNodeCoaxPort
IMPORTANT: The Forward
Label you type while creating the relationship must match the EsriDesignName
entry in the Schema.xml file for this component.
|
|
Backward Label |
SECom.ARCFM.RFNode |
|
Message Direction |
None (no messages propagated) |
|
Cardinality |
1–M (one to many) |
|
Relationship Attributes |
No, I do not want to add attributes to this relationship class |
|
Primary Key |
NetworkId |
|
Foreign Key |
NodeId |