MultiSessionOperationTrigger
Node Action:
This node action is used in the entry node of a workflow to specify that when multiple sessions are selected in the Session Manager window, a button appears in the list of buttons under the Multiple Session Selected section that triggers the workflow when clicked.
Parameters:
se_type
MultiSessionOperationTrigger
se_type = MultiSessionOperationTriggerse_visibilityCondition
se_visibilityCondition = "(ctx, log)
=> { return false; }"Contains code that must return a bool indicating when the workflow button should be visible
in the respective list of buttons in Session Manager.
se_displayName
The display name of the workflow button in Session Manager.
se_iconUrl
The URL for the icon of the workflow button in Session Manager.
se_iconService
The service for the icon of the workflow button in Session Manager.
se_iconXaml
se_iconXaml = "
<Canvas
Width=\"20\"
Height=\"20\"
Margin=\"1\"
SnapsToDevicePixels=\"True\">
<!-- Insert Icon Components -->
</Canvas>
"
The XAML for the icon of the workflow button in Session Manager.
se_sortOrder
The order in which the workflow button appears in the list of buttons in Session Manager.
se_showButtonText
Indicates whether the button text should show in the Session Manager window.
Example:
Multi Session Operation without Icon: This example illustrates how to properly use the MultiSessionOperationTrigger node action when no icon is specified.
digraph workflow {
entry[
label = "Reassign Button"
se_type0 = MultiSessionOperationTrigger
se_displayName0 = "Reassign With Reason"
se_sortOrder0 = 10
se_visibilityCondition0 = "(ctx, log) => {
return ((IEnumerable<dynamic>)ctx.Event.assignments).All(a => a.assignedTo == ctx.User.UserId) && ctx.Event.isSessionOpen == false;
}"
]
exit[
shape = invhouse,
color = "#22FF44",
style = filled
]
entry -> exit
}