ZoomTo
Node Action:
This node action zooms to a specified bounding box on the active map in ArcGIS Pro.
Parameters:
se_type
ZoomTo
se_type = ZoomTose_determineBoundingBox
se_typedetermineBoundingBox = "(ctx,
log) => { return ctx.State.MapExtent.extent; }"Contains code to determine which bounding box is zoomed to.
Example:
Zoom To Session Bounds: This example determines the bounds of the active session and uses that as the bounding box to zoom to on the active map.
digraph workflow {
entry[
se_type0 = SessionToolTrigger,
se_displayName0 = "Zoom To Session Boundary"
se_iconUrl0 = "https://mysubscription.blob.core.windows.net/img/extenticon.png",
se_sortOrder0 = 100,
se_visibilityCondition0 = "(ctx, msLogger) => {
return true;
}"
]
getSessionBounds[
se_type0 = Action,
se_action0 = "(ctx, msLogger) => {
ctx.State.SessionBounds = new List<dynamic>(ctx.Event.assignment.bounds).Any() ? ctx.Event.assignment.bounds : ctx.Event.session.sessionBounds;
}",
se_type1 = CopyToClipboard,
se_determineData1 = "(ctx, msLogger) => {
return JsonConvert.SerializeObject(ctx.State.SessionBounds);
}"
]
zoomToSessionBounds[
se_type0 = ZoomTo,
se_determineBoundingBox0 = "(ctx, log) => {
return JsonConvert.SerializeObject(ctx.State.SessionBounds);
}",
]
entry->getSessionBounds->zoomToSessionBounds->exit
}