RefreshAvailableJobsList
Node Action:
This node action refreshes the list of available jobs for the user's current operational map.
Parameters:
se_type
RefreshAvailableJobsList
se_type = RefreshAvailableJobsListExample:
Complete Current Assignment: This example refreshes both the My Jobs and Available Jobs lists in Session Manager, and completes the current assignment.
digraph workflow {
entry[
se_type0 = CompleteAssignmentTrigger,
se_displayName0 = "Complete Assignment "
se_iconUrl0 = "https://mysubscription.blob.core.windows.net/img/funnyassignmenticon.png"
se_requiresConnection0 = false,
se_sortOrder0 = 100,
se_visibilityCondition0 = "(ctx, log) => {
return ctx.Event.assignment.assignedTo == ctx.User.UserId && ctx.Event.isSessionOpen == true;
}"
]
notifyUser[
se_type0 = NotifyUser,
se_determineMessage0 = "(dynamicStateMachineContext, msLogger) => {
return \"Completed Selected Assignment\";
}",
se_notificationType0 = "Information",
se_showToast0 = true
]
refreshUI[
se_type0 = RefreshMyJobsList,
se_type1 = Timer,
se_delay1 = 200,
se_type2 = RefreshAvailableJobsList,
se_type3 = Timer,
se_delay3 = 200,
]
exit[
se_type0 = Action,
se_action0 = "(ctx, log) => {
string acceptanceStatus;
if (AssignmentTypeEquals(\"Approval\") || AssignmentTypeEquals(\"Review\"))
{
acceptanceStatus = \"Approved\";
}
else
{
acceptanceStatus = \"NotApplicable\";
}
ctx.Output.Cancel = false;
ctx.Output.WorkflowButtonKey = \"Send\";
ctx.Output.ShouldCloseSession = true;
ctx.Output.AcceptanceStatus = acceptanceStatus;
ctx.Output.WatchForAssignmentType = null;
ctx.Output.Reason = null;
ctx.Output.UserId = null;
bool AssignmentTypeEquals(string assignmentType)
=> assignmentType.Equals((string)ctx.Event.assignment.assignmentType,
StringComparison.InvariantCultureIgnoreCase);
}"
se_type1 = CopyToClipboard,
se_determineData1 = "(ctx, msLogger) => {
return JsonConvert.SerializeObject(ctx.Output);
}"
]
entry->notifyUser->refreshUI->exit
}