SessionToolTrigger
Node Action:
This node action is used in the entry node of a workflow to specify that when a single session is selected in the Session Manager window, a button appears in the list of buttons under the Tasks section that triggers the workflow when clicked.
Parameters:
se_type
SessionToolTrigger
se_type = SessionToolTriggerse_visibilityCondition
se_visibilityCondition = "(ctx, log)
=> { return false; }"Contains code that must return a bool indicating when the workflow button should be visible
in the respective list of buttons in Session Manager.
se_displayName
The display name of the workflow button in Session Manager.
se_iconUrl
The URL for the icon of the workflow button in Session Manager.
se_iconService
The service for the icon of the workflow button in Session Manager.
se_iconXaml
se_iconXaml = "
<Canvas
Width=\"20\"
Height=\"20\"
Margin=\"1\"
SnapsToDevicePixels=\"True\">
<!-- Insert Icon Components -->
</Canvas>
"
The XAML for the icon of the workflow button in Session Manager.
se_sortOrder
The order in which the workflow button appears in the list of buttons in Session Manager.
se_showButtonText
Indicates whether the button text should show in the Session Manager window.
Example:
Session Tool without Icon: This example illustrates how to properly use the SessionToolTrigger node action where no icon is defined.
digraph workflow {
entry[
se_type0 = SessionToolTrigger,
se_displayName0 = "Session Tool #1",
se_sortOrder0 = 1000,
se_visibilityCondition0 = "(ctx, msLogger) => {
return true;
}",
]
exit[
shape = invhouse,
color = "#22FF44",
style = filled
]
entry -> exit
}