SessionManagerToolTrigger
Node Action:
This node action is used in the entry node of a workflow to specify that a button should appear in the list of buttons under the drop-down in the active jobs list tab that triggers the workflow when clicked.
Parameters:
se_type
SessionManagerToolTrigger
se_type = SessionManagerToolTriggerse_visibilityCondition
se_visibilityCondition = "(ctx, log)
=> { return false; }"Contains code that must return a bool indicating when the workflow button should be visible
in the respective list of buttons in Session Manager.
se_displayName
The display name of the workflow button in Session Manager.
se_iconUrl
The URL for the icon of the workflow button in Session Manager.
se_iconService
The service for the icon of the workflow button in Session Manager.
se_iconXaml
se_iconXaml = "
<Canvas
Width=\"20\"
Height=\"20\"
Margin=\"1\"
SnapsToDevicePixels=\"True\">
<!-- Insert Icon Components -->
</Canvas>
"
The XAML for the icon of the workflow button in Session Manager.
se_sortOrder
The order in which the workflow button appears in the list of buttons in Session Manager.
se_showButtonText
Indicates whether the button text should show in the Session Manager window.
Example:
Session Manager Tool with Icon Xaml: This example illustrates how to properly use the SessionManagerToolTrigger node action, where the icon is defined by XAML.
digraph workflow {
entry[
se_type0 = SessionManagerToolTrigger,
se_displayName0 = "Session Manager Tool #1"
se_sortOrder0 = 0,
se_iconXaml0 = "
<Canvas
Width=\"20\"
Height=\"20\"
Margin=\"1\"
SnapsToDevicePixels=\"True\">
<Path
Data=\"M 10,4 10,16\"
Stroke=\"{StaticResource SE_DarkGreenBrush}\"
StrokeEndLineCap=\"Round\"
StrokeStartLineCap=\"Round\"
StrokeThickness=\"4\" />
<Path
Data=\"M 4,10 16,10\"
Stroke=\"{StaticResource SE_DarkGreenBrush}\"
StrokeEndLineCap=\"Round\"
StrokeStartLineCap=\"Round\"
StrokeThickness=\"4\" />
<Path Stroke=\"{StaticResource SE_DarkGreenBrush}\" StrokeThickness=\"1\">
<Path.Data>
<EllipseGeometry
Center=\"10,10\"
RadiusX=\"10\"
RadiusY=\"10\" />
</Path.Data>
</Path>
</Canvas>
",
se_visibilityCondition0 = "(ctx, log) => {
return true;
}",
]
exit[
shape = invhouse,
color = "#22FF44",
style = filled
]
entry -> exit
}