SessionOperationTrigger
Node Action:
This node action is used in the entry node of a workflow to specify that when a single session is selected in the Session Manager window, a button appears in the list of buttons above the Session Details tab that triggers the workflow when clicked.
Parameters:
se_type
SessionOperationTrigger
se_type = SessionOperationTriggerse_visibilityCondition
se_visibilityCondition = "(ctx, log)
=> { return true; }"Contains code that must return a bool indicating when the workflow button should be visible
in the respective list of buttons in Session Manager.
se_displayName
The display name of the workflow button in Session Manager.
se_isPrimaryOperation
Indicates whether the workflow represents a primary session operation. If true, the workflow is executed upon session 'double-click' or from the session drop-down list on the Session Manager ribbon.
se_sortOrder
The order in which the workflow button appears in the list of buttons in Session Manager.
Example:
Session Operation with Icon Xaml: This example illustrates how to properly use the SessionOperationTrigger node action where the icon is defined by XAML.
digraph workflow {
entry[
label = "Session Operation #1 Button"
se_type0 = SessionOperationTrigger
se_isPrimaryOperation0 = true,
se_displayName0 = "Session Operation #1",
se_sortOrder0 = 10,
se_showButtonText0 = false,
se_visibilityCondition0 = "(ctx, log) => {
return ctx.Event.assignment.assignedTo == ctx.User.UserId &&
(ctx.Event.isSessionOpen == null || ctx.Event.isSessionOpen == false);
}",
se_iconXaml0 = "
<Canvas
Width=\"32\"
Height=\"32\"
SnapsToDevicePixels=\"True\">
<Path
Data=\"M 1.0857284,26.93696 V 4.4772093 h 9.1557426 l 1.885006,2.5267215 16.426478,0.1403736 v 3.2285896\"
Fill=\"{StaticResource SE_SkyBlueBrush}\"
Stroke=\"{DynamicResource SE_DarkGrayBrush}\"
StrokeEndLineCap=\"Round\"
StrokeMiterLimit=\"1.0\"
StrokeStartLineCap=\"Round\"
StrokeThickness=\"2.0\" />
<Path
Data=\"M 31.245822,11.074762 26.937236,27.217706 1.0857284,27.077332 6.2021726,11.074762 H 31.111178\"
Fill=\"{DynamicResource SE_WhiteBrush}\"
Stroke=\"{DynamicResource SE_DarkGrayBrush}\"
StrokeEndLineCap=\"Round\"
StrokeMiterLimit=\"1.0\"
StrokeStartLineCap=\"Round\"
StrokeThickness=\"2.0\" />
</Canvas>"
]
exit[
shape = invhouse,
color = "#22FF44",
style = filled
]
entry -> exit
}