Field Mapping

Fiber facilities that have ports (patch panels, devices, splitters, etc.) follow a grid configuration to determine the location of each port.

For example, a patch panel card might have 24 ports. But, how are they arranged? Is is 12 x 2? 6 x 4? 8 x 3? The answer lies in the grid configuration, not just for the card, but for all the parent devices as well.


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?