Wavepoint XI Implementation

ArcFM Wavepoint XI is an extension of ArcFM Fiber Manager XI. Prior to implementing and configuring Wavepoint XI, you need to implement and configure Fiber Manager XI. See the Fiber Manager XI Implementation Guide for more information.


Roles and Scopes

When you are configuring Group Membership for Fiber Manager XI make sure you create the applicable roles required for Wavepoint XI.

If you access both Fiber Manager XI and Wavepoint XI, you must have the Fiber.Viewer role to access and use Wavepoint XI.

The roles of Fiber.Editor and Fiber.Admin are not authorized to access and use Wavepoint XI.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?