Configure Wavepoint XI

Wavepoint XI is an extension of Fiber Manager XI. Wavepoint XI’s configuration occurs within Solution Center > Fiber Manager.


To navigate to the configuration pages, follow these steps:

  1. In Solution Center, click Fiber Manager.

  2. On the Feature Services tab, choose the appropriate feature service from the menu.

  3. Click the Wavepoint tab.

  4. On the left side, click each section to configure it.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?