Measure Tool

The Measure tool on the Wavepoint XI toolbar lets you measure the distance between points in segments and in total distance.

To measure the distance between points on the map, click the Measure tool, then click the first point on the map. Move the curser to the next point. Continue to add points around the map until done. You can change the units the distance is reported in as required.

IMPORTANT: The reported distance in the tool is cumulative of all the points.

You can print out the results of any measurement with the Print option.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?