Fiber Manager Reporting

Fiber Manager provides the ability to generate XML- or HTML-based reports that graphically display information about your fiber optic network. You can generate the following reports with Fiber Manager:

IMPORTANT: At this time, Internet Explorer is the only browser supported by Fiber Manager.

  • The Allocation Report allows you to graphically view all of the connected fibers within a fiber optic cable.

  • The Fiber Trace Report graphically displays the results of a Fiber, OTDR, or Circuit trace. The format of the reports vary by trace type.

  • The Glass Report displays an inventory of the fiber optic cables in your network.

  • The Patch Panel Connection Report creates a graphical diagram of the layout of a patch panel or series of patch panels within a patch location.

  • The Splice Report presents a display of every fiber connection within the selected splice point.

  • The Cable Report presents the wavelengths, circuits, and statuses of circuits on the selected cable.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.